Everything

r_iwdt_iwuni_interrupt

Performs processing in response to the non-maskable/maskable interrupt.

Remark         This API function is called to run interrupt processing for the non-maskable / maskable interrupt, which is generated when the down-counter underflows or refreshing proceeds.

 

[Syntax]

static void    r_iwdt_iwuni_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.