The Code Generator is used to change the creation date into the file header of the source code by selecting [Code Generator Setting] tab >> [Generate File Mode] >> [Creation date] in the Property panel.
![](r20ut3104ej0110_cscgpf-25.gif)
The Code Generator is used to change the creation date into the file header of the source code by selecting [Code Generator Setting] tab >> [Generate File Mode] >> [Creation date] in the Property panel.