Everything
2.6.1 Change output format

The Code Generator is used to change the output format (HTML file or CSV file) of the report file by selecting [Code Generator Setting] tab >> [Generate File Mode] >> [Report type] in the Property panel.

Figure 2.16

Change Output Format

 

Remark

The output format of the report file is selected from the two types shown below.

HTML file

Outputs in the HTML format.

CSV file

Outputs in the CSV format.