The Peripheral Functions panel is opened to set the information necessary to control the peripheral functions (clock generator, pin functions, etc.) provided in the device.
To open the Peripheral Functions panel, double-click [Project name (Project)] >> [Code Generator (Design Tool)] >> [Peripheral Functions] (>> Peripheral function node) in the Project Tree panel.
![](r20ut3104ej0110_cscgpf-1.gif)
If an unsupported device is defined in the project for Code Generator, then ”[Code Generator (Design Tool)] node” will hide under [Project name (Project)] in the Project Tree panel. |