Everything
2.3.1 Input rule

Following is the rules for input to the Peripheral Functions panel.

(1)

Character set

Character sets that are allowed to input are as follows.

ASCII

1-byte alphabet, number, symbol

Shift-JIS

2-byte alphabet, number, symbol, Hiragana, Katakana, Kanji and 1-byte Katakana

EUC-JP

2-byte alphabet, number, symbol, Hiragana, Katakana, Kanji and 1-byte Katakana

UTF-8

2-byte alphabet, number, symbol, Hiragana, Katakana, Kanji (include Chinese character) and 1-byte Katakana

 

(2)

Number

Notations allowed when entering numbers are as follows.

Decimal number

A numeric value that starts with a number between 1 and 9 and followed by numbers between 0 and 9, and the numeric value 0

Hex number

A numeric value that starts with 0x and followed by a combination of numbers from 0 to 9 and characters from A to F (characters are not case sensitive)