20.19	 Cyclic Handler Information (cyclic_hand[])
 Here, each cyclic handler is defined.
 
 Parentheses < >show the user input part. 
 
 -	 Description
Define the cyclic handler ID number.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 1 to 255
 
 -	 When omitting
The cfg600px assigns the ID number automatically.
 
 -	 Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
 
 #define   <ID name>   <ID number>
 -	 Definition format
Symbol
 
 -	 When omitting
Cannot be omitted.
 
 3 )	 Cyclic handler entry address (
entry_address)
 
 -	 Description
Define the starting function of the cyclic handler.
 
 -	 Definition format
Symbol
 
 -	 When omitting
Cannot be omitted.
 
 4 )	 Activation cycle (
interval_counter)
 
 -	 Description
Define the activation cycle in millisecond.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 1 to (0x7FFFFFFF - system.tic_nume) / system.tic_deno
 
 -	 When omitting
The set value in the default system configuration file (factory setting: 1) applied.
 
 5 )	 Initial state (
start)
 
 -	 Description
Define the initial state of the cyclic handler.
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 OFF:	Non operational stat (The TA_STA attribute is not specified.)
 
 ON:	Operational state (The TA_STA attribute is specified.)
 
 -	 When omitting
The set value in the default system configuration file (factory setting: "OFF") applied.
 
 6 )	 Activation phase (
phs_counter)
 
 -	 Description
Define the activation phase in millisecond
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 0 to 
interval_counter
 
 -	 When omitting
The set value in the default system configuration file (factory setting: 0) applied.
 
 7 )	 TA_PHS attribute (
phsatr)
 
 -	 Description
Define the attribute concerning the activation phase.
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 OFF:	Not preserve the activation phase. (The TA_PHS attribute is not specified.)
 
 ON:	Preserve the activation phase. (The TA_PHS attribute is specified.)
 
 -	 When omitting
The set value in the default system configuration file (factory setting: "OFF") applied.
 
 8 )	 Extended information (
exinf)
 
 -	 Description
Define the extended information of the cyclic handler.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 0 to 0xFFFFFFFF
 
 -	 When omitting
The set value in the default system configuration file (factory setting: 0) applied.
 
 -	 Note
The extended information is passed to the cyclic handler.