-   
 
   ref_mpf
   iref_mpf
  
    -   
  
 
 Reference fixed-sized memory pool state.
 
 ER      ref_mpf (ID mpfid, T_RMPF *pk_rmpf);
 ER      iref_mpf (ID mpfid, T_RMPF *pk_rmpf);
 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 ID      mpfid;
 
 | 
    
 ID number of the fixed-sized memory pool.
  
 | 
  
  
    | 
 | 
    
 T_RMPF  *pk_rmpf;
 
 | 
    
 Pointer to the packet returning the fixed-sized memory pool state.
  
 | 
  
 
 [Fixed-sized memory pool state packet: T_RMPF]
 
 
  
  
    
 typedef struct  t_rmpf {
     ID      wtskid;         /*Existence of waiting task*/
     UINT    fblkcnt;        /*Number of free memory blocks*/
 } T_RMPF;
 
 | 
  
 
 Stores fixed-sized memory pool state packet (ID number of the task at the head of the wait queue, number of free memory blocks, etc.) of the fixed-sized memory pool specified by parameter 
mpfid in the area specified by parameter 
pk_rmpf.
 
 -	 
wtskid
Stores whether a task is queued to the fixed-size memory pool.
 
 Value:	ID number of the task at the head of the wait queue
 
 -	 
fblkcnt
Stores the number of free memory blocks.
 
 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 Note	 When the iref_mpf is issued from task or the ref_mpf is issued from non-task, the context error is not detected and normal operation of the system is not guaranteed.
  
 | 
  
  
    | 
 | 
    
 | 
    
 Memory access violation. (only for ref_mpf)
  
 -	 The operand-write access to the area indicated by  pk_rmpf has not been permitted to the invoking task.
  
 | 
  
  
    | 
 | 
    
 | 
    
 -	 The fixed-sized memory pool specified by  mpfid does not exist.
  
 |