Defines the stack size for a symbol.
[Syntax]
|
Symbol field
|
Mnemonic field
|
Operand field
|
Comment field
|
|
.stack
|
symble-name=value
|
[; comment]
|
[Function]
- | Defines the stack size to be shown in Call Walker for a symbol. |
[Description]
- | This defines the stack size to be shown in Call Walker for a symbol. |
- | The stack size for a symbol can only be defined once, and subsequent definitions are ignored. |
- | The stack size can only be defined as a 4-byte range of 0x0 to 0xFFFFFFFC. If a different value is specified, then the definition is ignored. |
[Remark]
- | See the user's manual of CS+ for details about Call Walker. |