This option enables the source-code checking of the MISRA-C:2004 rules or MISRA-C: 2012 rules, which are partially suppressed by the extended language specifications.
The source-code checking of the MISRA-C:2004 rules or MISRA-C: 2012 rules is disabled, which are partially suppressed by the extended language specifications.
This option enables the source-code checks of the MISRA-C:2004 rules or MISRA-C: 2012 rules in the following cases where they are suppressed by the unique language specifications extended from the C language standard.  | 
When the function has no prototype declaration (rule 8.1) and #pragma interrupt is specified for it.  | 
This option is valid only when the -misra2004 or -misra2012 option is specified.  | 
To enable the source-code checking of the MISRA-C:2004 rules, which are partially suppressed by the extended language specifications, describe as:  |