This option specifies link options.
[Specification format]
 
-  | Interpretation when omitted  | 
 
Only the link options specified by the compilation driver are passed to the optimizing linker.
[Detailed description]
-  | This option passes arg to the optimizing linker as the link option.  | 
 
-  | An error will occur if arg is omitted.  | 
 
[Example of use]
-  | To pass the -form=relocate option to the optimizing linker, describe as:  | 
 
>ccrl -lnkopt=-form=relocate -cpu=S2 -dev=dr5f100pj.dvf main.c 
 | 
 
 
The -lnkopt option specified in the above example has the same effect as the following example.
>ccrl -c -cpu=S2 -dev=dr5f100pj.dvf main.c 
>rlink -form=relocate main.obj 
 |