This section explains options for the assemble phase.
Caution about options are shown below.
When numerical values are specified as parameters, hexadecimal numbers which starts with "0x" ("0X") or decimal numbers can be specified.  | 
When a file name is specified as a parameter, it can include the path (absolute path or relative path).  | 
When a parameter includes a space (such as a path name), enclose the parameter in a pair of double quotation marks (").  | 
When the -prn_path, -mirror_source, -mirror_region, -define, -undefine, -include, -base_number, -warning, or -no_warning option is specified for ccrl command, the -asmopt option must be used.  | 
The types and explanations for options are shown below.