This option disables checking of the address to which the section is allocated.
[Specification format]
 
-  | Interpretation when omitted  | 
 
Whether sections are allocated to memory as shown below is checked, and if they are not allocated so, an error will occur.
| 
 | 
 | 
| 
 
.option_byte 
 | 
 
Address is fixed 
 | 
| 
 
.security_id 
 | 
 
Address is fixed 
 | 
| 
 
.sbss / .sdata 
 | 
 
saddr area 
 | 
| 
 
.sbss / .sdata (RAM side when the -rom option is specified) 
 | 
 
saddr area 
 | 
| 
 
.bss / .data 
 | 
 
Internal RAM 
 | 
| 
 
.bss / .data (RAM side when the -rom option is specified) 
 | 
 
Internal RAM 
 | 
| 
 
.const 
 | 
 
Flash mirror space 
 | 
| 
 
.constf 
 | 
 
Internal ROM 
 | 
| 
 
.sdata / .data (ROM side when the -rom option is specified) 
 | 
 
Internal ROM 
 | 
| 
 
.text 
 | 
 
Program memory 
 | 
| 
 
.text_unit64kp / .textf 
 | 
 
Program memory 
 | 
 
[Detailed description]
-  | This option disables checking whether the memory location that is read from the device file is consistent with the memory location of the section.  | 
 
[Example of use]
-  | To disable checking of the address to which the section is allocated, describe as:  | 
 
>rlink a.obj b.obj -no_check_section_layout 
 | 
 
[Remark]
-  | If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid.  |