Everything

-create_unfilled_area


< Optimizing Linkage Editor (rlink) Options / Output Options >

[Format]

-create_unfilled_area

[Description]

-

This option is available in V2.03 and later versions of this compiler.

-

When a Motorola S-record file (<name>.mot) or Hex file (<name>.hex) is output, this option blocks spaces created by .OFFSET directives in the assembly language being filled with output data.

-

When using this option, specify it when using the ccrx or asrx command to create an object file (<name>.obj) as well as when using the rlink command to create a Motorola S-record file or Hex file.