Everything
3.1.2 Object Information

Figure 3.1 shows an example of object information output.

* RX FAMILY ASSEMBLER V2.00.00  [15 Feb 2013] *  SOURCE LIST  Mon Feb 18 20:15:19 2013
(1)      (2)               (3)   (4)
LOC.     OBJ.              0XMDA SOURCE STATEMENT
 
                                 ;RX Family C/C++ Compiler (V2.00.00  [15 Feb 2013])  18-Feb-2013 20:15:19
                                 
                                 ;*** CPU TYPE ***
                                 
                                 ;-ISA=RXV1
                                 
                                 ;*** COMMAND PARAMETER ***
                                 
                                 ;-output=src=sample.src
                                 ;-listfile
                                 ;-show=source
                                 ;sample.c
                                 
                                 		.glb	_x
                                 		.glb	_func02
                                 		.glb	_func03
                                 		.glb	_func01
                                 (5)      (6)
                                 ;LineNo. C-SOURCE STATEMENT
                                 
                                 		.SECTION	P,CODE
00000000                         _func02:
                                 		.STACK	_func02=12
                                 ;       1 #include "include.h"
                                 ;       2 int func01(int);
                                 ;       3 int func03(int);
                                 ;       4 
                                 ;       5 int func02(int z)
00000000 6E67                    		PUSHM R6-R7
00000002 EF16                    		MOV.L R1, R6
                                 ;       6 {
                                 ;       7     x = func01(z);
00000004 05rrrrrr             A  		BSR _func01
00000008 FB72rrrrrrrr            		MOV.L #_x, R7
0000000E E371                    		MOV.L R1, [R7]
                                 ;       8     if (z == 2) {
00000010 6126                    		CMP #02H, R6
00000012 18                   S  		BNE L12
00000013                         L11:	; bb3
                                 ;       9         x++;
00000013 6211                    		ADD #01H, R1
00000015 08                   S  		BRA L13
00000016                         L12:	; bb6
                                 ;      10     } else {
                                 ;      11         x = func03(x + 2);
00000016 6221                    		ADD #02H, R1
00000018 39rrrr               W  		BSR _func03
0000001B                         L13:	; bb13
0000001B E371                    		MOV.L R1, [R7]
                                 ;      12     }
                                 ;      13     return x;
                                 ;      14 }
0000001D 3F6702                  		RTSD #08H, R6-R7
00000020                         _func03:
                                 		.STACK	_func03=4
                                 ;      15 
                                 ;      16 int func03(int p)
                                 ;      17 {
                                 ;      18     return p+1;
00000020 6211                    		ADD #01H, R1
                                 ;      19 }
00000022 02                      		RTS
                                 		.SECTION	D,ROMDATA,ALIGN=4
00000000                         _y:
00000000 01000000                		.lword	00000001H

.END

Item Number

Description

(1)

Location information (LOC.)

Location address of the object code that can be determined at assembly.

(2)

Object code information (OBJ.)

Object code corresponding to the mnemonic of the source code.

(3)

Line information (0XMDA)

Results of source code processing by the assembler. The following shows the meaning of each symbol.

0

X

M

D

A

Description

0-30

 

 

 

 

Shows the nesting level of include files.

 

X

 

 

 

Shows the line where the condition is false in conditional assembly when -show=conditions is specified.

 

 

M

 

 

Shows the line expanded from a macro instruction when -show=expansions is specified.

 

 

D

 

 

Shows the line that defines a macro instruction when -show=definitions is specified.

 

 

 

S

 

Shows that branch distance specifier S is selected.

 

 

 

B

 

Shows that branch distance specifier B is selected.

 

 

 

W

 

Shows that branch distance specifier W is selected.

 

 

 

A

 

Shows that branch distance specifier A is selected.

 

 

 

 

*

Shows that a substitute instruction is selected for a conditional branch instruction.

(4)

Source information (SOURCE STATEMENT)

Contents of the assembly-language source file.

(5)

C/C++ source line number (LineNo.)

(6)

C/C++ source statement (C-SOURCE STATEMENT)

C/C++ source statement output when the -show=source option is specified.