Everything
3.3.1 Structure of Library List

Table 3.4 shows the structure and contents of the library list.

Table 3.3

Structure and Contents of Library List

No

Output Information

Contents

SuboptionNote

When -show Option is not Specified

1

Option information

Option strings specified by a command line or subcommand

-

Output

2

Error information

Error messages

-

Output

3

Library information

Library information

-

Output

4

Information of modules, sections, and symbols within library

Module within the library

-

Output

When show=symbol is specified:
List of symbol names in a module within the library

-show=symbol

Not output

When show=section is specified:
Lists of section names and symbol names in a module within the library

-show=section

Not output

Note

All options are valid when the -list option is specified.