Everything
8.5.5 Combinations of Code Generating Options

When the master and application are built, the option settings related to the PIC/PID function should be matched between the objects that compose the master and application.

The following shows the rules for specifying options for each object compilation and the conditions of option settings in other objects that can be linked.

(1)

Master

When building the master, specify the PIC/PID function options as shown in Table 8.6.

Table 8.6

Rules for Specifying PIC/PID Function Options in Master

Option Name

For Compilation

Conditions on Setting the Option for Linkable Objects

pic

× Not allowed

pic is not specified

pid

× Not allowed

pid is not specified

nouse_pid_register

O Can be specified except the standard library and setting PID register of the startup program

No conditions

fint_register

O Can be specified

fint_register with the same parameters must be specified

base

O Can be specified

base with the same parameters must be specified

(2)

Application

When building an application, specify the PIC/PID function options as shown in Table 8.7.

Table 8.7

Rules for Specifying PIC/PID Function Options in Application

Option Name

For Compilation

Conditions on Setting the Option for Linkable Objects

pic

O Can be specified

pic is necessary

pid

O Can be specified

pid is necessary

nouse_pid_register

× Not allowed

nouse_pid_register is not specified

fint_register

O Can be specified

fint_register with the same parameters must be specified

base

O : Can be specified

base* with the same parameters must be specified

Note

* When pid is specified, base=rom=<register> is not allowed.

(3)

Between Master and Application

In the master and application, the PIC/PID function options should be specified as shown in tTable 8.8.

Table 8.8

Rules for Combinations of PIC/PID Function Options between Master and Application

Options in Application

Options in Master

pic

No conditions

pid

nouse_pid_register is necessary if application calls functions of master

fint_register

fint_register with the same parameters is necessary

base

base* with the same parameters is necessary

Note

* When pid is specified, base=rom=<register> is not allowed.