Everything
2.15.4.3 Edit a Point Trace event

Detailed information on a Point Trace event is edited in the Detailed Settings of Point Trace dialog box. This dialog box is opened by selecting the Point Trace event you desire to edit on the Events panel then selecting [Edit Condition...] from the context menu.

(1)

When editing an address condition

The compare condition, address and address mask can be specified as an address condition in the Detailed Settings of Point Trace dialog box.

(2)

When editing an data condition

The access type, access size, compare condition, compare data and data mask can be specified as an data condition in the Detailed Settings of Point Trace dialog box.

(3)

When editing an pass count condition [Simulator]

The pass count can be specified as an pass count condition in the Detailed Settings of Point Trace dialog box.

(4)

When editing an event target [Full-spec emulator][E1][E20]

The following can be specified as an event target in the Detailed Settings of Point Trace dialog box.

Event Target

Function

CPU

Access to the CPU is the target of the point trace (default).

Global RAM

Access to the Global RAM is the target of the point trace.

Cluster RAM

Access to the Cluster RAM is the target of the point trace.