Everything
2.16.2.4 Delete a Timer Result event

To delete a Timer Result event you have set, on the Editor panel/Disassemble panel, right-click the event mark in the event area and select [Delete Event] from the context menu that is displayed.

Also, there is another way to delete a set event. Select the Timer Result event you want to delete on the Events panel, and then click the button in the toolbar (see "2.20.5 Delete events").

Caution

[Simulator]
If either a timer start or timer end event is deleted from the event marks on the event area, all of the corresponding event marks are deleted.