Everything
2.17.1 Measure the performance in a section

In the program execution process, the performance in a section can be measured by setting a Performance Measurement event.

To use this function, follow the procedure described below.

 

2.17.1.1 Set a Performance Measurement event

2.17.1.2 Execute the program

2.17.1.3 Edit a Performance Measurement event

2.17.1.4 Delete a Performance Measurement event

Caution

Also see "2.20.7 Notes for setting events" for details on Performance Measurement events (e.g. limits on the number of enabled events).