Everything
2.20.3 Jump to the event address

Clicking the following buttons jumps to each panel which selected events address exist.

Note however, that when a Trace event/Timer Result event/Performance Measurement event/Unconditional Trace event/Run-Break Timer event is selected, these buttons are disabled.

 

Opens the Editor panel and jumps to the source line corresponding to the address where the selected event is being set.

 

Opens the Disassemble panel and jumps to the disassemble results corresponding to the address where the selected event is being set.

 

Opens the Memory panel and jumps to the source line corresponding to the address where the selected event is being set.