2.15.3
Collect execution history in a section
The execution history is collected as trace data only for a section while the program is in execution by setting a Trace event.
This Trace event consists of a trace start event and a trace end event.
To use this function, follow the procedure described below.
2.15.3.1 Set a Trace event
2.15.3.2 Execute the program
2.15.3.3 Edit a Trace event
2.15.3.4 Delete a Trace event
Caution 2. | [Simulator]
Trace start events and trace stop events cannot be set/deleted while a tracer is running. |
Caution 3. | [Simulator]
If you perform a trace from a trace start event until a trace end event, the simulator will not include the trace end event in the results of the trace. For this reason, if you are using a simulator, set the trace end event one line below the range for which you require display of the trace data. |