2.22.3 Icons for invalid input
In some of the dialog boxes in CS+, the
icon will appear at a point where incorrect characters are entered as a warning sign.
Remark | Placing the cursor over the
icon will pop up the information that indicates the characters to be entered. |