The source file is displayed in the Editor panel below. The Editor panel automatically opens with displaying source text of the specified position (see "2.7.1 Execute downloading") when a load module file is successfully downloaded.
If you want to open the Editor panel manually, double-click on the source file in the Project Tree panel.
For details on the contents and function in each area, see the section for the Editor panel.