2.8.2.2
Change display format
The display format of the disassemble area can be changed using buttons below on the toolbar.
|
View
|
The following buttons to change the display format are displayed.
|
|
|
Show Offset
|
Displays the offset value of the label. The offset value from the nearest label is displayed when a label is defined for the address.
|
|
Show Symbol
|
Displays the address value as the result of disassembling in the format "symbol + offset value" (default).
Note that when a symbol has been defined as the address value, only the symbol is displayed.
|
|
Show Function Name
|
Displays the name of the register by its function name (default).
|
|
Show Absolute Name
|
Displays the name of the register by its absolute name.
|