Everything
2.8.4.2 Edit code

Follow the steps below to edit code.

(1)

Switch to edit mode

Double-click the code to edit or select [Edit Code] from the context menu after moving the caret to the code to edit.

(2)

Edit code

Use keyboard to directly edit the code.

(3)

Write to memory

Press the [Enter] key to write the code to the memory after editing.

If the edited instruction is invalid, the instruction is shown in red and will not be written to the memory.

When the code is written to the memory, the result of disassembling is also updated.