To reset CPU, click the
button on the debug toolbar.
When CPU is reset, the current PC value is set to the reset address.
You can automatically overwrite the value of I/O register/CPU register with the specified values after CPU reset under breaking (see "2.21 Use Hook Function" for details). |
The [Reset While Running] category on the [Debug Tool Settings] tab of the Property panel |