Everything
2.12.2 Stop the program manually

The program in execution is forcibly stopped by clicking the button on the debug toolbar (Forced break function).

Remark

In cases of failure to stop a program during execution, the following setting may be required to allow stopping execution of the program.
However, stopping a program while this setting is in place leads to a CPU reset.

-

The [Reset While Running] category on the [Debug Tool Settings] tab of the Property panel

[Use the force reset] property

[Yes]