The execution history is collected as trace data only for a section while the program is in execution by setting a Trace event.
This Trace event consists of a trace start event and a trace end event.
To use this function, follow the procedure described below.
| Also see "2.15.7 Notes for setting events" for details on Trace events (e.g. limits on the number of enabled events). | 
| The event type (execution type/access type) that can be set as trace start and end events differ with each debug tool used. | 
| [Simulator] | 
| [Simulator] |