Everything
2.9.2 Display/change the CPU register

The contents of the CPU register (general-purpose register/control register) can be shown and the value can be changed in the CPU Register panel below.

Select the [View] menu >> [CPU Register].

For details on the contents and function in each area, see the section for the CPU Register panel.

Figure 2.103

Display the Contents of CPU Register (CPU Register Panel)

(1): [Register Name] area

(2): [Value] area

 

This section describes the following.

 

2.9.2.1 Change display format of values

2.9.2.2 Modify the CPU register contents

2.9.2.3 Display/modify the CPU register contents during program execution

2.9.2.4 Save the CPU register contents