Everything
2.18.2 Input signals to the pins

To configure the input signal to a pin, click the on the Simulator GUI window's toolbar. The following Signal Data Editor window opens.

You can use this window to set the input signal data for the input pin to a numerical value, to be input at an arbitrary time.

See the section on the Signal Data Editor window for details about controlling the window.

Figure 2.177

Configuring Input Signal to Pin (Signal Data Editor Window)