CS+ is an integrated developing environment platform for RH850 family, RX family, V850 family, RL78 family, 78K0R microcontroller and 78K0 microcontroller.
CS+ comprehensively supports the operations required for program development such as designing, coding, building, debugging, and flash programming.
In this manual, the debugging is explained out of those operations needed for the program development.
| When the E2 emulator Lite (abbreviated name: E2 Lite) is used, please read references to "E1" in this manual as also meaning "E2 Lite". | 
Among them, this manual focuses on the description of debugging the outline of which is provided in this chapter.