Everything
 

Jump to Function dialog box


This dialog box is used to select a function to be jumped if there are some functions with the same names when a program jumps to the function specified on the Editor panel.

Caution 1.

This dialog box is displayed only when there are some functions with the same names and also [Yes(-Xcref)][CC-RH][CC-RX]/[Yes(-cref)][CC-RL] is specified with the [Output cross reference information] property on the Property panel of the build tool to be used.

Caution 2.

This dialog box targets only files that have been registered in the project.

Figure A.14

Jump to Function Dialog Box

 

This section describes the following.

[How to open]

-

On the Editor panel, select [Jump to Function] from the context menu.

[Description of each area]

(1)

Candidates in the jump destination display area

This area displays a list of candidates in the jump destination.

Candidates are displayed in the alphabetical order of the names of [File]. If candidates are included in the same file, they are displayed in the order of line numbers.

(a)

[File Name]

Displays the name of the file (without any path) in which the function is defined.

(b)

[Line Number]

Displays the number of the line to which the function is defined.

(c)

[Path]

Displays the path of the file in which the function is defined.

[Function buttons]

Button

Function

OK

Jumps to the line that defines the target function after selecting the line in Candidates in the jump destination display area and clicking this button.

Cancel

Cancels the jump and closes this dialog box.

Help

Displays the help for this dialog box.