Q0120000 |
[Message] |
The following updates must be installed to install the updates you selected. Do you want to select these updates? |
Q0120004 |
[Message] |
The following installations were suspended. Do you want to resume installation? |
Q0120005 |
[Message] |
There are suspended installations. Close the following applications before resuming the installations.
The application may display the icon in the notification area (system tray).
xxx |
Q0120006 |
[Message] |
Administrative privileges is required to run the updates. Do you want to acquire administrative privileges to continue updates? If you select [Yes], the dialogue for acquire the administrative privileges will be displayed. |
Q0130001 |
[Message] |
Do you want to delete files corresponding to the selected updates? |
Q0140006 |
[Message] |
Multiple information files used to update and obtain information about the software were found on your computer.
Do you want to replace these files with the information file that is included in the product being installed?
Select 'Yes' to replace the files and continue the installation.
Select 'No' to cancel the installation now. |
Q0140007 |
[Message] |
A different version of the information file used to update and obtain information about the software was found on your computer.
Do you want to replace the file with the information file that is included in the product being installed?
Select 'Yes' to replace the file and continue the installation.
Select 'No' to keep the original file and continue the installation. |
Q0140011 |
[Message] |
Are you sure you want to cancel the installation? |
[Explanation] |
This appears when [Cancel] is clicked on a wizard page. |
Q0140035 |
[Message] |
The following applications in the installation folder are running.
Close these applications and click Retry to continue.
The application may display the icon in the notification area (system tray).
- xxx
- xxx
- xxx |
[Explanation] |
This appears when a CS+-associated tool is running while the integrated installer/uninstaller is being operated. |
Q0140045 |
[Message] |
Are you sure you want to cancel the installation?
The following products installation has been completed.
- xxx
:
Please install the latest service packs and security updates for this product using
Windows Update and Microsoft Update. |
[Explanation] |
This message appears when all installation of required environments has completed successfully without a reboot request, and the user then clicks [Cancel] in the windows of the integrated installer that is executed subsequently. |
Q0200001 |
[Message] |
Continue the processing? |
[Explanation] |
This message appears to confirm whether to proceed with a given action. |
[Action by User] |
[OK]:
Continue action.
[Cancel]:
Cancel action. |
Q0200002 |
[Message] |
You need to restart this product to take effect.
Do you want to restart now? |
[Explanation] |
This appears when confirming a reboot. |
[Action by User] |
[Yes]:
Continue action.
[No]:
Cancel action. |
Q0200003 |
[Message] |
Are you sure you want to close? |
[Explanation] |
This message appears when confirming the closure of some window/dialog box. (If closure is selected, the data being displayed will be discarded.) |
[Action by User] |
[OK]:
Close the window/dialog box.
[Cancel]:
Do not Close the window/dialog box. |
Q0200004 |
[Message] |
Are you sure you want to back? |
[Explanation] |
This message appears when confirming the return from some processing. (If return is selected, the data being displayed will be discarded.) |
[Action by User] |
[OK]:
Return.
[Cancel]:
Do not Return. |
Q0201001 |
[Message] |
xxx has been changed. Save? |
[Explanation] |
This Message dialog box appears to confirm whether you want to save a changed file when closing a window or the like.
"xxx" is replaced by the display name of the open window (file name or panel name).
When closing a project, "xxx" is replaced by "Project".
If there are two or more items, this string is changed to "Items" |
[Action by User] |
[Yes]:
Save the content before closing the window or panel.
[No]:
Discard any changes and close the window or panel.
[Cancel]:
Stay in current state, without closing the window. |
Q0201002 |
[Message] |
xxx may have been changed by another program. Overwrite save? |
[Explanation] |
This message appears when saving a file, and for some reason the last modified date is more recent than the time the file was opened or the time of the last save. |
[Action by User] |
[Yes]:
Overwrite and save.
[No]:
Cancel action. |
Q0201003 |
[Message] |
Folder does not exist. Create folder? |
[Explanation] |
This appears to ask the user whether to create a folder when creating a file, if the specified path includes a folder that does not exist. |
[Action by User] |
[Yes]:
Create the folder.
[No]:
Close the dialog box. |
Q0201004 |
[Message] |
The file already exists. Overwrite? |
[Explanation] |
This message is used in various dialog boxes that have a filename field. |
[Action by User] |
[Yes]:
Overwrite the file.
[No]:
Return the focus to the original dialog box, without overwriting the file. |
Q0201005 |
[Message] |
Save all the files currently being edited? |
[Explanation] |
This message appears to ask the user whether to save files being edited. |
[Action by User] |
[Yes]:
Save all the files currently being edited.
[No]:
Cancel action. |
Q0201006 |
[Message] |
If the registered files opened by some external tools, exit that tools. To continue the processing, press [OK]. |
[Explanation] |
This message appears to ask the user whether to save files being edited by an external tool. |
[Action by User] |
[Yes]:
Continue the processing.
[No]:
Cancel action. |
Q0201007 |
[Message] |
xxx may have been changed by another program. Are you sure you want to reload the file? |
[Explanation] |
This appears when changes have been made to the file (edits, deletions, or renaming). |
[Action by User] |
[Yes]:
Reload the file.
[No]:
Cancel action. |
Q0201008 |
[Message] |
The file(xxx) already exists. Overwrite? |
[Explanation] |
This message appears in order to confirm with the user whether to overwrite a file that has already been saved. |
[Action by User] |
[Yes]:
Overwrite the file.
[No]:
Return the focus to the original dialog box, without overwriting the file. |
Q0201009 |
[Message] |
The folder(xxx) already exists. Overwrite? |
[Explanation] |
This message appears in order to confirm with the user whether to overwrite a folder that has already been saved. |
[Action by User] |
[Yes]:
Overwrite the folder.
[No]:
Return the focus to the original dialog box, without overwriting the folder. |
Q0201010 |
[Message] |
Are you sure you want to change the file extension?
If the file extension is changed, any settings of the file will be deleted. |
[Explanation] |
This message appears to confirm that you wish to change the file extension in the project tree. |
[Action by User] |
[Yes]:
Change the file extension.
[No]:
Cancel action. |
Q0202001 |
[Message] |
Saving the project components may take a few minutes to a few dozen minutes. Start processing? |
[Explanation] |
This appears when the [Save Project and product name as Package] menu item is selected. |
[Action by User] |
[Yes]:
Execute processing.
[No]:
Cancel action. |
Q0202002 |
[Message] |
Could not find the project file. Unregist the corresponding project from the list of favorite project? |
[Explanation] |
This appears when selecting a project from favorites, and the project file does not exist. |
[Action by User] |
[Yes]:
Delete project.
[No]:
Do nothing. |
Q0202003 |
[Message] |
Are you sure you want to import build options?
Current whole build options and build modes are replaced by specified project values. |
[Explanation] |
This appears when selecting the [Import Build Options...] menu. |
[Action by User] |
[Yes]:
The import of the build options begins.
[No]:
Cancel action. |
Q0202004 |
[Message] |
xxx is not a project for the yyy.
Do you want to reopen this project by the proper CS+ and close this product?
If [No] is selected, restore only file structure on this product and you can not build and debug the project. |
[Explanation] |
This appears when attempting to load a project from another package. |
[Action by User] |
[Yes]:
Re-open this project by the proper CS+.
[No]:
Open this project by the current CS+.
[Cancel]:
Cancel action. |
Q0202005 |
[Message] |
xxx is not a project for the yyy.
Are you sure you want to just open the project?
If you just open the project, only file structure will be restored, and you will not be able to build and debug the project.
If you would like to build and debug, open the project by the proper CS+. |
[Explanation] |
This appears when attempting to load a project from another package. |
[Action by User] |
[OK]:
Open this project by the current CS+.
[Cancel]:
Cancel action. |
Q0202006 |
[Message] |
xxx is not a subproject for the yyy.
Are you sure you want to just open the subproject?
If you just open the subproject, only file structure will be restored, and you will not be able to build and debug the project.
If you would like to build and debug, open the subproject by the proper CS+. |
[Explanation] |
This appears when attempting to add a sub-project from another package. |
[Action by User] |
[OK]:
Add a subproject by the current CS+.
[Cancel]:
Cancel action. |
Q0202007 |
[Message] |
xxx
This project file may have been changed by another program. Would you like to reload the main project? |
[Explanation] |
This message appears when external update of the project file is detected. |
[Action by User] |
[Yes]:
Reload the main project.
[No]:
Do nothing. |
Q0203001 |
[Message] |
Are you sure you want to set the current compile options to the individual compile options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This appears when specifying the individual compile options. |
[Action by User] |
[Yes]:
The individual compiler options are set for all build mode.
[No]:
The individual compiler options are only set for the current build mode.
[Cancel]:
Cancel action. |
Q0203002 |
[Message] |
Are you sure you want to set the current assemble options to the individual assemble options for all build modes? |
[Explanation] |
This appears when specifying the individual assemble options. |
[Action by User] |
[Yes]:
The individual compiler options are set for all build mode.
[No]:
The individual compiler options are only set for the current build mode.
[Cancel]:
Cancel action. |
Q0203003 |
[Message] |
Are you sure you want to copy the current compile options to the assemble options for all build modes? |
[Explanation] |
This appears when the [Build simultaneously] property on the [Common Options] tabbed page is changed from [Yes] to [No]. |
[Action by User] |
[Yes]:
The compiler options are copied to all build mode.
[No]:
The compiler options are only copied to the current build mode.
[Cancel]:
Cancel action. |
Q0203004 |
[Message] |
It may not be built properly because a circular reference exists.
Continue the processing? |
[Explanation] |
This message appears when there is a circular reference between projects. |
[Action by User] |
[Yes]:
Execute Build/Clean.
[Cancel]:
Cancel Build/Clean. |
Q0203005 |
[Message] |
Are you sure you want to set the current compile options to the individual assemble options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This message appears when individual assemble options are specified (with simultaneous build enabled). |
[Action by User] |
[Yes]:
The individual compiler options are set for all build mode.
[No]:
The compiler options are only copied to the current build mode.
[Cancel]:
Cancel action. |
Q0203006 |
[Message] |
Are you sure you want to apply the setting value to all build modes?
If [No] is selected, apply to the current build mode only. |
[Explanation] |
This message appears when build options for all build modes are changed in a batch. |
Q0203007 |
[Message] |
The specified build mode name already exists.
Are you sure you want to overwrite it? |
[Explanation] |
This message appears when a build mode of the same name already exists. |
[Action by User] |
[OK]:
Overwrite the build mode.
[Cancel]:
Do not overwrite the build mode. |
Q0204001 |
[Message] |
Hot Plug-in is prepared.
Connect the debug target to a PC and click OK. |
[Explanation] |
This message appears while waiting for the connection of a hot plug-in. |
[Action by User] |
[Yes]:
Continue the processing.
[No]:
Cancel action. |
Q0204002 |
[Message] |
Load module file xxx has changed. Do you want to download it again? |
[Explanation] |
This appears when [Observe downloaded load module files changing] is enabled, and the load module file is modified. |
[Action by User] |
[Yes]:
The download is executed.
[No]:
Cancel action. |
Q0206001 |
[Message] |
No data corresponding to the search conditions was found. Search from xxx of the specified range? |
[Explanation] |
This appears in the Message dialog box when no results were found for the search parameters in the Memory Search or Trace Search dialog box. xxx will be either "start" or "end" |
[Action by User] |
[Yes]:
Close the Message dialog box and perform the search again from the beginning of the range.
[No]:
Close the Message dialog box and move the focus to the original dialog box. |
Q0210001 |
[Message] |
End debugging by disconnecting from the debug tool? |
[Explanation] |
- | When closing the Main window while connected to the debugging tool, a confirmation Message dialog box appears, asking the user whether to disconnect the debugging tool. |
- | This message appears when closing a project while connected to the debugging tool. |
- | This message appears when opening a project or making it newly while connected to the debugging tool. |
|
[Action by User] |
[Yes]:
Disconnect and close the window.
[No]:
Close the window without disconnecting.
[Cancel]:
Cancel closing the Main window. |
Q0210002 |
[Message] |
Also change the security ID of the debug tool? |
[Explanation] |
In the Build Tool, when the [Security ID] property is changed, this message asks whether to also change the security ID of the debugging tool. |
[Action by User] |
[Yes]:
Change the security ID of the debug tool.
[No]:
Cancel action. |
Q0210004 |
[Message] |
Also change the programmable I/O area start address of the debug tool? |
[Explanation] |
In the Build Tool, when the [Programmable I/O area start address] property is changed, this message asks whether to also change the Programmable I/O area start address of the debugging tool. |
[Action by User] |
[OK]:
Change the programmable I/O area start address of the debug tool.
[Cancel]:
Cancel action. |
Q0210005 |
[Message] |
Are you sure you want to clear all coverage information? |
[Explanation] |
This appears when coverage information is cleared. |
[Action by User] |
[OK]:
Clear all coverage information.
[Cancel]:
Cancel action. |
Q0210006 |
[Message] |
Also change the endianness of the debug tool? |
[Explanation] |
This appears when the endian property setting is changed in the build tool, and the application asks whether you want to change the endian property setting also in the debugging tool. |
[Action by User] |
[OK]:
Change the endianness of the debug tool.
[Cancel]:
Cancel action. |
Q0210007 |
[Message] |
Also enable the trace function of a debugging tool? |
[Explanation] |
This appears when the trace RAM warning property setting is changed in the build tool, and the application confirms whether you want to change the enable trace property setting in the debugging tool as well. |
[Action by User] |
[OK]:
Enable the trace function of a debugging tool.
[Cancel]:
Cancel action. |
Q0210008 |
[Message] |
Also disable the trace function of a debugging tool? |
[Explanation] |
This appears when the trace RAM warning property setting is changed in the build tool, and the application confirms whether you want to change the enable trace property setting in the debugging tool as well. |
[Action by User] |
[OK]:
Disable the trace function of a debugging tool.
[Cancel]:
Cancel action. |
Q0212001 |
[Message] |
The I/O protection area has been set in the specified target memory area. Also delete the I/O protection area? |
[Explanation] |
This message appears when removing a target memory area, and an I/O protected area has been set on this area. |
[Action by User] |
[OK]:
Delete the I/O protection area.
[Cancel]:
Cancel action. |
Q0225001 |
[Message] |
All the property values on this sheet are reset to the default values. OK? |
[Explanation] |
The program asks for user confirmation when the [Property]->[Reset All to Default] command is executed. |
[Action by User] |
[Yes]:
The property values are reset to the default values.
[No]:
Cancel action. |
Q0232001 |
[Message] |
Delete build mode xxx? |
[Explanation] |
This message appears when attempting to delete a build mode. |
[Action by User] |
[OK]:
Delete build mode xxx.
[Cancel]:
Cancel action. |
Q0232002 |
[Message] |
Requires saving the current project to enable to restore the current project status after changing the microcontroller.
Continue saving and processing? |
[Explanation] |
This appears when the microcontroller is changed. |
[Action by User] |
[OK]:
Continue saving and processing.
[Cancel]:
Cancel action. |
Q0261001 |
[Message] |
The section has been set the specified segment. Also delete the section? |
[Explanation] |
This appears when deleting a segment, and the segment to be deleted held one or more sections. |
[Action by User] |
[Yes]:
Delete the entire section.
[No]:
Cancel delete. |
Q0261002 |
[Message] |
The memory space has been set the specified memory area. Also delete the memory area and segment that includes? |
[Explanation] |
This message appears when a memory area is included in the memory space that is to be deleted. |
[Action by User] |
[Yes]:
Delete the entire memory area.
[No]:
Cancel delete. |
Q0261003 |
[Message] |
The memory area has been set the specified segment. Also delete the segment? |
[Explanation] |
This message appears when a segment is included in the memory area that is to be deleted. |
[Action by User] |
[Yes]:
Delete the entire memory area.
[No]:
Cancel delete. |
Q0261004 |
[Message] |
Some of the segments that are set in the memory area that have changed, fall outside the range of address. Continue saving and processing?
(If you continue, the start address of the segment is outside the range will be empty) |
[Explanation] |
This message appears when some of the segments in the memory area that has been changed are located outside the specified address range. |
[Action by User] |
[Yes]:
Apply the change. The addresses of the segments located outside the specified address range will be blank.
[No]:
Cancel the change. |
Q0262001 |
[Message] |
This product recommends that creating project at the same place as the original project folder. Are you sure you want to change the project folder?
Selected folder : xxx
Recommended folder(diverted project folder) : yyy
* Build error may be occurred in the creating project. Because, the folder for a creating project is different from the original. |
[Explanation] |
In the Create Project dialog box, if the source and destination project folders are different, and source conversion is to be performed, then you will be asked to confirm whether to perform the operation. |
[Action by User] |
[Yes]:
Change the creating folder to original project folder, proceed to source conversion.
[No]:
Without changing the creating folder, proceed to source conversion.
[Cancel]:
Return to the Create Project dialog box, and do not proceed to source conversion. |
Q0268001 |
[Message] |
Open the CubeSuite project without changing the settings?
If you select [No], open a dialog to change other device or other compiler. |
[Explanation] |
This appears when an old CubeSuite product (.cspj) is specified in [Open Project...]. |
[Action by User] |
[Yes]:
The .cspj is opened as if it were a .mtpj file.
[No]:
The Project Conversion Settings dialog box opens. Specify the device, project name, and other properties for conversion.
[Cancel]:
The message dialog box closes, and the opening of the CubeSuite project is cancelled. |
Q0268002 |
[Message] |
A non-empty folder is specified. If you just convert project to the folder, to backup all files in the folder, it may take a long time to copy the files.
Do you want to create a sub folder named with the project name?
If [Yes] is selected, CS+ will create the folder and convert the project to the folder to prevent a large-amount copy. However, when there is path settings based on the project folder in Additional include paths and so on, it is necessary to change them after conversion. |
[Explanation] |
This message appears if the [Backup the project composition after before conversion] check box is selected, the conversion source pass differs from the conversion destination pass, and the folder specified as the destination of conversion is not empty when converting a project in the Project Convert Setting dialog box. |
[Action by User] |
[Yes]:
Create a sub folder named with the project name in the destination folder of conversion, then execute conversion.
[No]:
Execute conversion without any other processes.
[Cancel]:
Close the message and abort the project conversion processing. |
Q0269001 |
[Message] |
The specified name already exists in the list. Are you sure you want to save it with the specified name?
If you select "Yes", save it with duplicated name. |
[Explanation] |
This message appears when the profile result is saved regardless of the same item name already existing. |
[Action by User] |
[Yes]:
Save the profile result under the specified name.
[Cancel]:
Do not save the profile result.
Re-open the Character String Input dialog box to input the name. |
Q0269002 |
[Message] |
The specified name already exists in the list. Are you sure you want to rename it with the specified name?
If you select "Yes", rename it with duplicated name. |
[Explanation] |
This message appears when the profile result is renamed regardless of the same item name already existing. |
[Action by User] |
[Yes]:
Rename the profile result under the specified name.
[Cancel]:
Do not rename the profile result. |
Q0271001 |
[Message] |
Are you sure you want to override quality records data? |
[Explanation] |
This message appears to confirm if you wish to overwrite an existing file of quality-related information. |
[Action by User] |
[OK]:
The file will be overwritten.
[Cancel]:
The file will not be overwritten (and no data will be output). |
Q0271002 |
[Message] |
Do you want to open the output folder in Explorer? |
[Explanation] |
This message appears after the output of a file of quality-related information. |
[Action by User] |
[OK]:
The folder will be opened in Windows File Explorer.
[Cancel]:
The folder will not be opened in Windows File Explorer. |
Q0272001 |
[Message] |
Do you refresh the contents of display? |
[Explanation] |
This message appears when you have switched between regions. |
[Action by User] |
[OK]:
The contents of tables will be refreshed.
[Cancel]:
The contents of tables will not be refreshed. |
Q0272002 |
[Message] |
The Smart Browser has a new notification with high importance.
Click [Yes] to view. |
[Explanation] |
This message appears when an important notification (an item with the [High] mark against it) is added to the [Notifications] tab on the [Smart Browser] panel. |
[Action by User] |
[Yes]:
A notification regarding the item is displayed in the Smart Browser.
[No]:
Do nothing and close the dialog box. |
Q0291001 |
[Message] |
Do you change a file extension? |
[Explanation] |
[RH850][RX] This message appears when [Type of output file] property in [Output] category in [Link Options] tab will change the file extension of the output file.
[RL78] This message appears when [Hex file format] property in [Hex Format] category in [Hex Output Options] tab will change the file extension of the output file. |
[Action by User] |
[Yes]:
Change the output file extension.
[No]:
Do not change the output file extension. |
Q0291002 |
[Message] |
The folder already contains the following file(s):
xxx
Would you like to change the existing files to *.bak?
(Note: In the case of Yes, if *.bak files already exist they will be overwritten) |
[Explanation] |
This message appears when file of the same name as a startup program created when project is created already exists at the project creating folder. |
[Action by User] |
[Yes]:
Change the existing files to *.bak and create new files.
[No]:
Overwrite the existing files. |
Q0291003 |
[Message] |
All or part of the following useful settings for the memory mapping profile are not enabled. Would you like to enable these options?
In the [List] category of the [Link Options] tab,
* the [Outputs the linkage list file] property
* the [Outputs a symbol name list in a module] property
* the [Shows the total sizes of sections] property |
[Explanation] |
This message appears if the related options of the linker are not ON when the [Profile] button in the Memory Mapping Profiler panel is clicked and changed to the [Profile(Collect)] button (only the first time after the project is opened). |
[Action by User] |
[Yes]:
Change the options of the linker to ON and collect memory mapping information.
[No]:
Collect memory mapping information without changing the options of the linker. |
Q0291005 |
[Message] |
For the [Uses double-precision floating-point operation instructions] property, -dpfpu is selected.
Would you like to change [Uses double-precision floating-point operation instructions] to "No" and set -nofpu? |
[Explanation] |
This message appears if you have selected an option that is not available when [No] has been selected for [Uses single-precision floating-point operation instructions] in the build properties of CC-RX. |
Q0293001 |
[Message] |
You are making the level 3 (inter-module optimization) setting.
For reasons of safety, individual compiler and assembler options become invalid at level 3. The object and library files you have registered will also become invalid (but can be re-set).
The libraries added to the [Using libraries] property will also be removed. See the [All Messages] tab in the Output panel.
Do you wish to continue with the setting? |
[Explanation] |
This appears when you have selected whole-program optimization (-Xwhole_program) in build properties, to confirm whether you really want to select this option. |
[Action by User] |
[Yes]:
This disables individual options, removes user-registered obj and lib files from the project, and enables -Xwhole_program.
[No]:
This restores the property selections, clearing the -Xwhole_program option. |
Q0293003 |
[Message] |
Are you sure you want to set the current compile options to the individual compile options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This message appears when individual compile options are specified. |
[Action by User] |
[Yes]:
The individual compiler options are set for all build mode.
[No]:
Apply the current compile options to the individual compile options for the current build mode only.
[Cancel]:
Cancel action. |
Q0293004 |
[Message] |
Are you sure you want to set the current assemble options to the individual assemble options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This message appears when individual assemble options are specified. |
[Action by User] |
[Yes]:
The individual compiler options are set for all build mode.
[No]:
Apply the current compile options to the individual compile options for the current build mode only.
[Cancel]:
Cancel action. |
Q0293005 |
[Message] |
Are you sure you want to copy the current compile options to the assemble options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This message appears when the [Build simultaneously] property on the [Common Options] tabbed page is changed from [Yes] to [No]. |
[Action by User] |
[Yes]:
The compiler options are copied to all build mode.
[No]:
Copy the current compile options to the assemble options for the current build mode only.
[Cancel]:
Cancel action. |
Q0293006 |
[Message] |
Are you sure you want to set the current compile options to the individual assemble options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This message appears when individual assemble options are specified (with simultaneous build enabled). |
[Action by User] |
[Yes]:
The compiler options are copied to all build mode.
[No]:
Copy the current compile options to the assemble options for the current build mode only.
[Cancel]:
Cancel action. |
Q0293007 |
[Message] |
On the [Output Code]/[Default section of data area] property, ep_disp16 or ep_disp23 is selected.
Would you like to change [Default section of data area] to "Not specify(None)" and set [Optimize accesses to external variables]? |
[Explanation] |
This message appears when [Optimize accesses to external variables] is selected and an option that cannot be specified simultaneously is selected. |
[Action by User] |
[Yes]:
Change the [Default section of data area] property to [Not specify(None)] and set [Optimize accesses to external variables].
[No]:
Do not set [Optimize accesses to external variables]. |
Q0293008 |
[Message] |
All or part of the following useful settings for the memory mapping profile are not enabled. Would you like to enable these options?
In the [List] category of the [Link Options] tab,
* the [Output link map file] property
* the [Output symbol information] property
* the [Output total sizes of sections] property |
[Explanation] |
This message appears if the related options of the linker are not ON when the [Profile] button in the Memory Mapping Profiler panel is clicked and changed to the [Profile(Collect)] button (only the first time after the project is opened). |
[Action by User] |
[Yes]:
Change the options of the linker to ON and collect memory mapping information.
[No]:
Collect memory mapping information without changing the options of the linker. |
Q0293010 |
[Message] |
On the [Output Code]/[Default section of const area] property, zconst or zconst23 is selected.
Would you like to change [Default section of const area] to "Not specify(None)" and set [Enable PIC and PIROD functions]? |
[Explanation] |
This message appears when the PIC and PIROD functions are selected and options that cannot be specified at the same time have been selected. |
Q0293011 |
[Message] |
On the [Output Code]/[Default section of data area] property, r0_disp16 or r0_disp23 is selected.
Would you like to change [Default section of data area] to "Not specify(None)" and set [Enable PID functions]? |
[Explanation] |
This message appears when the PID function is selected and options that cannot be specified at the same time have been selected. |
Q0293012 |
[Message] |
On the [Output Code]/[Default section of const area] property, pcconst16 or pcconst23 is selected.
Would you like to change [Default section of const area] to "Not specify(None)" and change [Enable PIC and PIROD functions] to "No"? |
[Explanation] |
This message appears when the PIC and PIROD functions are released and options that cannot be specified have been selected. |
Q0293013 |
[Message] |
On the [Use of r4 register] property, -r4=none is selected.
Would you like to change [Use of r4 register] to "GP-relative base register(None)" and set [Enable PID functions]? |
[Explanation] |
This message appears when the PID function is selected and options that cannot be specified have been selected. |
Q0293014 |
[Message] |
On the [Optimizes accesses to external variables] property, -map or -smap is selected.
Would you like to change [Optimizes accesses to external variablesr] to "No" and set [Enable PIC and PIROD functions]? |
[Explanation] |
This message is displayed when an option which is not specifiable is selected while the [Optimize accesses to external variables] property is selected. |
[Action by User] |
[Yes]:
The [Optimize accesses to external variables] property is changed to “No” and the PIC and PIROD functions are configured.
[No]:
The PIC and PIROD functions are not configured. |
Q0293015 |
[Message] |
On the [Optimizes accesses to external variables] property, -map or -smap is selected.
Would you like to change [Optimizes accesses to external variablesr] to "No" and set [Enable PID functions]? |
[Explanation] |
This message is displayed when an option which is not specifiable is selected while the [Optimize accesses to external variables] property is selected. |
[Action by User] |
[Yes]:
The [Optimize accesses to external variables] property is changed to “No” and the PID functions are configured.
[No]:
The PID functions are not configured. |
Q0293016 |
[Message] |
You are making the level 3 (inter-module optimization) setting.
For reasons of safety, individual compiler and assembler options become invalid at level 3. The object and library files you have registered will also become invalid (but can be re-set).
The libraries added to the [Using libraries] property will also be removed. See the [All Messages] tab in the Output panel.
[Build simultaneously] in the [Build Method] category on the [Common Options] tab will be changed to "Yes".
Do you wish to continue with the setting? |
[Explanation] |
This message appears to ask if you wish to enable inter-module optimization (by specifying -whole_program or -Xwhole_program) when simultaneous building is disabled in the build properties of CC-RH or CC-RX. |
[Action by User] |
[Yes]:
Inter-module optimization (level 3) is enabled. Individual compiler and assembler options will be disabled, object and library files that have been added will be removed, and simultaneous building will be re-enabled.
[No]:
This restores the property selections, clearing the Inter-module optimization (level 3). |
Q0294001 |
[Message] |
You are making the level 3 (inter-module optimization) setting.
For reasons of safety, individual compiler and assembler options become invalid at level 3. The object and library files you have registered will also become invalid (but can be re-set).
The libraries added to the [Using libraries] property will also be removed. See the [All Messages] tab in the Output panel.
Do you wish to continue with the setting? |
[Explanation] |
This is to confirm if you really wish to set the inter-module optimization (-Owhole_program) option as a build property of the CC-RL compiler. |
[Action by User] |
[Yes]:
Turn the individual options off, exclude obj/lib files added by the user, and turn -Owhole_program on.
[No]:
Ignore -Owhole_program and restore the previous property settings. |
Q0294003 |
[Message] |
Are you sure you want to set the current compile options to the individual compile options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This is to confirm the scope of individual compiler options when they are set. |
[Action by User] |
[Yes]:
Execute the command.
[No]:
Set the current compiler options for the current build mode only.
[Cancel]:
Cancel the command. |
Q0294004 |
[Message] |
Are you sure you want to set the current assemble options to the individual assemble options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This is to confirm the scope of individual assembler options when they are set. |
[Action by User] |
[Yes]:
Execute the command.
[No]:
Set the current assembler options for the current build mode only.
[Cancel]:
Cancel the command. |
Q0294005 |
[Message] |
Are you sure you want to copy the current compile options to the assemble options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This is to confirm changing of the value of the compiler option "Build simultaneously" from Yes to No. |
[Action by User] |
[Yes]:
Execute the command.
[No]:
Copy the current compiler options to the assembler options for the current build mode only.
[Cancel]:
Cancel the command. |
Q0294006 |
[Message] |
Are you sure you want to set the current compile options to the individual assemble options for all build modes?
If [No] is selected, copy the current build mode options only. |
[Explanation] |
This is to confirm the scope of individual assembler options when they are set (with simultaneous build enabled in CC-RL). |
[Action by User] |
[Yes]:
Execute the command.
[No]:
Copy the current compiler options to the individual assembler options for the current build mode only.
[Cancel]:
Cancel the command. |
Q0294007 |
[Message] |
All or part of the following useful settings for the memory mapping profile are not enabled. Would you like to enable these options?
In the [List] category of the [Link Options] tab,
* the [Output link map file] property
* the [Output symbol information] property
* the [Output total sizes of sections] property |
[Explanation] |
This message appears if the related options of the linker are not ON when the [Profile] button in the Memory Mapping Profiler panel is clicked and changed to the [Profile(Collect)] button (only the first time after the project is opened). |
[Action by User] |
[Yes]:
Change the options of the linker to ON and collect memory mapping information.
[No]:
Collect memory mapping information without changing the options of the linker. |
Q0294009 |
[Message] |
You are making the level 3 (inter-module optimization) setting.
For reasons of safety, individual compiler and assembler options become invalid at level 3. The object and library files you have registered will also become invalid (but can be re-set).
The libraries added to the [Using libraries] property will also be removed. See the [All Messages] tab in the Output panel.
[Build simultaneously] in the [Build Method] category on the [Common Options] tab will be changed to "Yes".
Do you wish to continue with the setting? |
[Explanation] |
This message appears to ask if you wish to enable inter-module optimization (by specifying -Owhole_program) when simultaneous building is disabled in the properties of the CC-RL compiler. |
[Action by User] |
[Yes]:
Inter-module optimization (level 3) is enabled. Individual compiler and assembler options will be disabled, object and library files that have been added will be removed, and simultaneous building will be re-enabled.
[No]:
This restores the property selections, clearing the Inter-module optimization (level 3). |
Q0300001 |
[Message] |
The pin is connected to the external peripheral <external peripheral name>. If you change the setting, the pin is disconnected. Do you want to change the setting? |
[Action by User] |
[Yes]:
Disconnect from the external peripheral and change the settings.
[No]:
Close the dialog box without changing the settings. |
Q0300002 |
[Message] |
The selected pin No. <selected pin No.> is used in <macro function>. Do you want to change the setting? |
[Action by User] |
[Yes]:
Change the settings.
[No]:
Close the dialog box without changing the settings. |
Q0300003 |
[Message] |
Deleting the column "<column name>". Continue? |
[Action by User] |
[Yes]:
Delete the column.
[No]:
Close the dialog box without deleting the column. |
Q0300004 |
[Message] |
Do you want to delete the external peripheral <external peripheral name>? If you delete the external peripheral, the pins connected to the external peripheral is disconnected. |
[Action by User] |
[Yes]:
Delete the external peripheral. Disconnect the pin.
[No]:
Return to the original status without changing the settings. |
Q0300005 |
[Message] |
All the settings you have done in the pin configurator will be lost. Do you want to change the package type? |
[Action by User] |
[Yes]:
This will modify the package. Pin settings and external peripherals will be returned to their default values.
[No]:
Return to the original status without changing the settings. |
Q0300006 |
[Message] |
Disconnecting the pin No. <selected pin number> from the external peripheral <external peripheral name>. Continue? |
[Action by User] |
[Yes]:
This disconnects the pin from the external periphery.
[No]:
Return to the original status without changing the settings. |
Q0300007 |
[Message] |
<File name> already exists. Do you want to replace it? |
[Action by User] |
[Yes]:
Overwrite save the file.
[No]:
Return to the original status without changing the settings. |
Q0300008 |
[Message] |
One or more pins are connected to the external peripheral(s). If you change the settings, the pins are disconnected. Do you want to change all settings? |
[Action by User] |
[Yes]:
Disconnect the pin connected to the external periphery, and change the settings.
[No]:
Return to the original status without changing the settings. |
Q0300009 |
[Message] |
One or more pins are used in other macro. Do you want to change all settings? |
[Action by User] |
[Yes]:
Change the settings of all pins, including those otherwise in use.
[No]:
Return to the original status without changing the settings. |
Q0404000 |
[Message] |
xxx has been changed. Save? |
Q0404001 |
[Message] |
Folder does not exist. Create a new folder? |
Q0404002 |
[Message] |
Do you want to save Code Generator setting? If 'No' is selected, Code Generator setting is not restored after this project is set to active project again. |
Q0615000 |
[Message] |
Also disable Access by stopping execution property of the debug tool? |
Q0615001 |
[Message] |
Also enable Access by stopping execution property of the debug tool? |
Q0615002 |
[Message] |
Also change Usage RAM monitoring and DMM by a debugging DTC system property of the debugtool? |
Q0801001 |
[Message] |
The file already exists. Overwrite? |
[Action by User] |
[Yes]:
Overwrite the file.
[No]:
Return the focus to the original dialog box, without overwriting the file. |
Q0810001 |
[Message] |
Discard analysis data and close the xxx panel of Program Analyzer to increase available memory? |
[Explanation] |
When the application runs out of memory during analysis, this appears to confirm whether to discard analysis results. |
[Action by User] |
[Yes]:
This discards the analysis results, freeing the memory and closing the analysis plug-in panel.
[No]:
This continues the task without discarding analysis results. Operation may become unstable from this point, because the application is working at the limits of memory capacity. |
Q0812001 |
[Message] |
The break point can be set to two or more addresses. Set the break point to all the addresses? |
[Explanation] |
This appears to confirm whether to set a break to all corresponding addresses when you have selected the [Set Break to Function] command, and the target function is a template function. |
[Action by User] |
[Yes]:
This sets break events to all addresses corresponding to the template function.
[No]:
This sets a break event only to address with the smallest value corresponding to the template function. |
Q0824001 |
[Message] |
No data corresponding to the search conditions was found. Is the search continued from the xxx? |
[Explanation] |
This appears when searching analysis graph value trends, and the specified value is not found in the direction of search.
"start" or "end" is displayed in xxx. |
[Action by User] |
[Yes]:
Close the Message dialog box and perform the search again from the beginning/end of the range.
[No]:
Close the Message dialog box and move the focus to the original dialog box. |
Q0824002 |
[Message] |
Restore the values of Variable/Address and Type/Size to the values before loading from a file? |
[Explanation] |
This appears when you have selected [Load from file] for the analyze tool's Property panel >> [Variable Value Changing] tab >> [Analysis method] property, and then changed to another method. It confirms whether to restore the property setting to the values before loading from file. |
[Action by User] |
[Yes]:
Discards the values loaded from file, and restores the previous values.
[No]:
Retains the values loaded from file. |
Q0824003 |
[Message] |
Registering watch-expressions currently being registered in the Watch panel (Watch1) as graphing target. If you continue, the information on the registered graphing targets will be deleted and the graph being displayed will be erased.
Continue the processing? |
[Action by User] |
[OK]:
Register watch expressions in the [Watch] panel as the targets for graphing.
[Cancel]:
Do nothing. |
Q0826001 |
[Message] |
When you save an image in this format may be very large file size. |
[Explanation] |
This warns that the size of the file is large, and confirms whether to really save it. |
[Action by User] |
[OK]:
Save the image.
[Cancel]:
Do nothing. |
Q1700000 |
[Message] |
The file xxx cannot be saved as it is Read Only.
Would you like to save the file as a different name or overwrite it? |
[Explanation] |
This message appears when a read-only file is to be overwritten. |
[Action by User] |
[Save As]:
Save the file as a different name.
[Overwrite]:
The attribute of the file is changed and it's overwritten.
[Cancel]:
Cancel action. |
Q1700512 |
[Message] |
A file with the name xxx already exists at the copy destination. Do you want to overwrite the file? |
Q2000001 |
[Message] |
The current editor file contains unsaved changes. You must save these changes first.xxxyyy. Would you like to save the changes to this file? |
[Explanation] |
This message dialog box appears when switching the Editor panel from source file view to mixed source view.
It is to inform the user that unsaved modifications have been made to the source file. The user must agree to save any modifications to the source file before source mixed mode can be displayed. |
[Action by User] |
[OK]:
The changes to the source file will be saved. If the changes are saved successfully then the editor view will continue to switch to source mixed view.
[Cancel]:
Cancel the operation of switching to source mixed view. The editor view will remain in source file view and the unsaved changes will remain. |
Q2000002 |
[Message] |
xxx has been changed. Save? |
[Explanation] |
This message dialog box appears to prompt to save any unsaved modifications to the Editor panel.
This prompt occurs when performing operations such as closing the Editor panel or reloading the current editor file. |
[Action by User] |
[Yes]:
This will save all unsaved modifications to the specified editor file.
[No]:
This will discard any unsaved modifications in the editor file.
[Cancel]:
This will cancel the operation that resulted in the prompt to save the file. The [Cancel] button may not be available if the save request is due to the application closing. |
Q2000004 |
[Message] |
The file xxx cannot be saved as it is Read Only. yyy Would you like to save the file as a different name or overwrite it? |
[Explanation] |
This message dialog box appears when attempting to save an editor source file that is read-only on disk. |
[Action by User] |
[Save As...]:
This will open a Save As dialog box to allow saving the file as a different file name.
[Overwrite]:
This will overwrite the existing read-only file. The read-only attribute will be changed to readable/writable.
[Cancel]:
This will cancel the operation that resulted in the prompt to save the file. |
Q2000005 |
[Message] |
xxxyyyzzz This file may have been changed by another program. Would you like to reload it? |
[Explanation] |
This message dialog box appears when a source file that is open in the editor has been modified externally in another application. |
[Action by User] |
[Yes]:
This will reload the editor source file, losing any unsaved modifications since the last save time of the file.
[No]:
This will ignore the external changes to the file, and will leave the Editor panel exactly as it is. Any unsaved changes will remain.
[Cancel]:
This will perform the same as the [No] button; ignoring any external changes to the file and leaving the Editor panel as it is. |
Q2000006 |
[Message] |
Generating a print image for large files may take a long time. Do you wish to continue? |
[Explanation] |
This message appears when the [Print...] or [Print Preview] menu was selected for a file with 1000 or more lines. |
[Action by User] |
[OK]:
An image is created.
[Cancel]:
Creation of an image is canceled. |
Q2000007 |
[Message] |
xxx file size is more than 24MB.
In the case of a large file, the processing of syntax coloring takes long time.
Disable the processing?
When syntax coloring is disabled, code outlining and smart editing also will be disabled.
Hereafter, this selection is applied to larger files than 24MB. |
[Explanation] |
This message appears to allow you to select whether to disable syntax coloring in a large file because of the time processing for this takes. |
[Action by User] |
[Yes]:
Syntax coloring, code outlining and smart edit function in files larger than 24 Mbytes is disabled.
[No]:
Syntax coloring, code outlining and smart edit function is always enabled. |
Q2200001 |
[Message] |
file-name is exist. overwrite? [y/n] |
[Explanation] |
The specified file already exists. |
[Action by User] |
[y]:
The file is overwritten and processing is continued.
[n]:
Cancel action. |
Q2300001 |
[Message] |
The file already exists. Overwrite? |
[Explanation] |
This message appears when there is a field to specify the file name in the dialog box. |
[Action by User] |
[Yes]:
Overwrite the file.
[No]:
Return the focus to the original dialog box, without overwriting the file. |