Everything
2. FUNCTIONS

This chapter describes the key functions provided by the Pin Configurator along with operation procedures.

Remark

In this chapter, an example where an RL78/G13 (ROM: 16KB) R5F1006A(20pin) is the target device is used to explain the key functions.