Everything

Editing the Program

2. Create a category

This section describes how to create a category.

Users can categorize files freely.

 

From the project tree, right click a file, then select [Add] → [Add New Category].

 

[New Category] is created as shown in the figure below. You can change the name to anything you like. As an example, here we name the category [Source File].

Drag [hwsetup.c], and drop it onto [Source Files]. [hwsetup.c] is now categorized as [Source Files].

We created two categories as an example.