You can save the execution results of the build (output messages of the build tool) that displayed on the Output panel.
Select the [Build Tool] tab on the panel, and then select [Save Output - Build Tool As...] from the [File] menu. The Save As dialog box will open.
![](ProjectOperation_Eng-117.gif)
In the dialog box, specify the file to be saved and then click the [Save] button.