Everything
2.3.10 Indicating mismatches between versions registered with the license manager and the floating license server

The balloon help that pops up from the icon indicates mismatches between versions registered with the license manager and the floating license server.

Figure 2.17

[Notification regarding the version of the license manager] Information Icon

 

Figure 2.18

[Notification regarding the version of the floating license server] Information Icon

 

Clicking on the icon or balloon help will produce a message dialog box.