Shows a list of panels and dialog boxes of the task analyzer tool below:
|
Displays analysis information such as execution transition state of the processing program, the state of real-time OS resource usage, and CPU usage status. The Analysis Result panel is displayed in the Child-panel display area on this panel. |
|
|
A child-panel of the Realtime OS Task Analyzer panel. This panel displays analysis information such as execution transition state of the processing program, the state of real-time OS resource usage, and CPU usage status. |
|
|
Specifies the type of the item to be displayed as a CPU usage status in the Analysis information table area on the Analysis Result panel. |
|
|
Sets filter conditions on the analysis information which is displayed as a CPU usage status in the Analysis information table area on the Analysis Result panel. |
|
|
Specifies the type of state line to be displayed as an execution transition state of the processing program, and whether an event mark is or is not to be displayed as a real-time OS resource usage status, in the Analysis information diagram area on the Analysis Result panel. |
|
|
Reads the analysis information that has been saved as the task analyzer trace data to display the information in the Child-panel display area on the Realtime OS Task Analyzer panel. |
|
|
Saves the analysis information that has been displayed in the Child-panel display area on the Realtime OS Task Analyzer panel as the task analyzer trace data. |