Everything
2.6.4 Sort the analysis information

You can sort the information values on the Function List panel/Variable List panel by column, and in ascending or descending order.

To do this, use the mouse to click the desired column name (clicking repeatedly toggles the sort order between ascending and descending).

If the items to sort are numbers (decimal or hexadecimal), then the information is sorted by numerical value. For other types of data (e.g. strings), the information is sorted by character code.

The following mark appears by the column name of the column that the information is sorted on:

Table 2.5

Marks that Indicate Sorted Display

Mark

Description

 

Indicates that the information is being sorted in ascending order.

Click again with the mouse to sort in descending order.

 

Indicates that the information is being sorted in descending order.

Click again with the mouse to sort in ascending order.

Remark

Click while holding down the [Shift] key to sort on multiple columns.