This dialog box is used to set modules which are output to the I/O header file.
![](Build-RH850_Eng-99.gif)
The following items are explained here.
On the Property panel, select the following property, and then click the [...] button. |
From the [I/O Header File Generation Options] tab, [Modules which are defined in device file] in the [I/O Header File] category |
This area displays a list of the names of modules defined in the device file and the names of the I/O header files to which the modules are output.
This area displays the names of modules which are defined in the device file.
If any of the check boxes is selected, the relevant module is output to the I/O header file shown under [File Name].
The check boxes are selected by default.
This area displays the names of the I/O header files to which the modules are output.
You can also directly enter a desired file name to change the I/O header file to which the module is output.
The default file name is “iodefine.h”.
This check box is used to select or deselect all of the check boxes under [Module Name].
If this check box is selected, check boxes under [Module Name] will all be selected.
If this check box is deselected, selection of the check boxes under [Module Name] will all be cleared.
When the same file name is specified for multiple modules, code for those modules is output to the same file. There is no case sensitivity for file names. |