Everything

-h


This option displays the descriptions of CcnvCA78K0R options.

[Specification format]

-h

 

-

Interpretation when omitted

The descriptions of CcnvCA78K0R options are not displayed.

[Detailed description]

-

This option outputs the descriptions of CcnvCA78K0R options to the standard error output.

-

Conversion is not performed when this option is specified.

-

When this option is specified simultaneously with another option, the other option is ignored.

-

When this option is specified simultaneously with the -V option, the -V option is given priority.

[Example of use]

>CcnvCA78K0R  -h