Everything
4.3 Information Types

When the message number type is information, the information types are classified as follows.

Table 4.2

Information Types

Information Type

Description

Change

Changes were made in the program so that it can be handled by the CC-RL.

Insert

Additions were made in the program so that it can be handled by the CC-RL.

Delete

Some descriptions were deleted because they are not necessary in the CC-RL.

Info

Conversion may not be sufficient in some cases because of the difference between the CA78K0R and CC-RL specifications.

Each case should be confirmed individually.