|
|
|
|
M0591111
|
Change
|
String1 was converted into string2.
|
The token was converted.
|
M0591112
|
Change
|
Bit access of I/O register was converted into macro call.
|
Since the bit access method of SFRs differs between the CA78K0R and CC-RL, the method is changed to make access using a macro.
|
M0591113
|
Change
|
'String' has been changed to syntax of CC-RL.
|
Since the description format differs between the CA78K0R and CC-RL, the description format is changed to that of the CC-RL.
|
M0591121
|
Insert
|
Inserted macro definition for bit access of I/O register.
|
Since the bit access method of SFRs differs between the CA78K0R and CC-RL, the method is changed to make access using a macro.
|
M0591122
|
Insert
|
Inserted #pragma interrupt NO_VECT.
|
#pragma interrupt without the vector table specification was generated.
|
M0591123
|
Insert
|
Inserted string.
|
A description in accordance with the CC-RL format was added.
|
M0591124
|
Insert
|
Add inline function string for assembly.
|
An inline function for assembly was generated.
|
M0591125
|
Insert
|
Inserted #pragma rtos_interrupt NO_VECT.
|
#pragma rtos_interrupt without the vector table specification was generated.
|
M0591131
|
Delete
|
String was deleted.
|
The description format is not available in the CC-RL. The description was deleted.
|
M0591141
|
Info
|
string1 was converted into string2.
But that cannot map in RAM.
|
Though the section of #pragma section was changed, there is a possibility that the section cannot be allocated. Check the user's manual of the CC-RL.
|
M0591142
|
Info
|
The section can not be converted. Because there is no matched section.
|
The section could not be converted because there is no corresponding section in the CC-RL.
|
M0591143
|
Info
|
Delete "AT start address".
|
This was deleted because an address cannot be specified by #pragma section in the CC-RL.
|
M0591144
|
Info
|
The MACRO cannot be converted. Because there is no matched macro.
|
The macro could not be converted because there is no corresponding macro in the CC-RL.
|
M0591145
|
Info
|
The label detected in the assembly code. Please correct label to appropriate content.
|
Only local labels can be written in an assembly-language function in the CC-RL. Modify the label to have suitable contents.
|