| R_ADCn_ADCSummation_Cannelm_GetResult | 
Reads the results of accumulation data.
[Syntax]
| void    R_ADCn_ADCSummation_Channelm_GetResult ( uint32_t * buffer ); | 
| 
Remark | n is the unit number, m is the channel number. | 
[Argument(s)]
|  |  |  | 
|  | uint32_t * buffer; | 
Pointer to area in which to store the results of accumulation data | 
[Return value]
None.