Start CSIG data reception.
| 
Remark 1. | This API function performs 2 byte-level CSIG reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf. | 
| 
Remark 2. | Starts after this API function is called, and R_CSIGm_Start is then called. | 
[Syntax]
| #include    "r_cg_macrodriver.h" MD_STATUS R_CSIGm_Receive ( const uint16_t * rx_buf, uint16_t rx_num ); | 
| 
Remark | m is the channel number. | 
[Argument(s)]
|  |  |  | 
|  | const uint16_t * rx_buf; | 
Pointer to a buffer to store the received data | 
|  | uint16_t rx_num; | 
Total amount of data to receive | 
[Return value]
|  |  | 
| 
MD_OK | 
Normal completion | 
| 
MD_ARGERROR | 
Invalid argument specification |