Performs processing in response to the OS timer interrupt.
Remark  | This API function is called as the interrupt process corresponding to the OS timer interrupt.  | 
 
[Syntax]
void    r_ostmm_interrupt ( void ); 
 | 
 
Remark  | m is the channel number.  | 
 
[Argument(s)]
None.
[Return value]
None.