3.2.18  
Peripheral Interconnection
 
Below is a list of API functions output by the Code Generator for peripheral interconnection use.
| 
Table 3.18 | API Functions: [Peripheral interconnection] | 
|  |  | 
| 
R_PICn_Create | 
Performs initialization necessary to control the peripheral interconnection functions. | 
| 
R_PICn_Create_UserInit | 
Performs user-defined initialization relating to the peripheral interconnection functions. | 
| 
R_PICn_Timer_SyncStart | 
Generates start triggers of the timers for which simultaneous start is enabled. |