Everything

R_12ADC_Set_ADChannel

Configures the analog voltage input pin for A/D conversion.

Remark         The value specified in argument channel is set to A/D channel select register A0 (ADANSA0) or A/D conversion extended input control register (ADEXICR).

 

[Syntax]

#include    "r_cg_macrodriver.h"

#include    "r_cg_12adc.h"

MD_STATUS    R_12ADC_Set_ADChannel ( ad_sel_regester_t regester, uint16_t data );

 

[Argument(s)]

I/O

Argument

Description

I

ad_sel_regester_t regester;

Set to selected register

SEL_ADANSA0  : A/D channel select register A0

                               (ADANSA0)

SEL_ADEXICR   : A/D conversion extended input control

                               register (ADEXICR)

I

uint16_t data;

Set to selected register value

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification