Everything

R_ADC_Start

Starts A/D conversion.

Remark         About 1 micro second of stabilization time is required when changing the voltage converter from operation stopped to operation enabled status.
Consequently, about 1 micro second must be left free between the call to
R_ADC_Set_OperationOn and the call to this API function.

 

[Syntax]

void       R_ADC_Start ( void );

 

[Argument(s)]

None.

 

[Return value]

None.