Everything

r_cgc_clockmonitor_interrupt

Performs processing in response to the clock monitor interrupt INTCLM.

Remark         This API function is called as the interrupt process corresponding to the clock monitor interrupt INTCLM.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_cgc_clockmonitor_interrupt ( void );

 

CC-RL Compiler

static void   __near r_cgc_clockmonitor_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.